REGEN.TESTVTHRESH

Description

This command is used to configure the timeout expected by the regen self-test feature. See REGEN.TEST for more info on how this timeout is used.

Versions

Action

Version

Notes

Implemented

02-07-03-000

General Information

Type

Read/Write

Units

Percent (%)

Range

60 to 99

Default Value

80

Data Type

Integer

See Also

REGEN.TEST
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
REGEN.TESTVTHRESH

3007h

0ah

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REGEN.TESTVTHRESH

2409

969

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.TESTVTHRESH

2409

Unsigned8

Read/Write

-